{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the largest amperage QO-GFI available?

Issue:
Maximum QO-GFI amperage

Product Line:
Miniature Circuit Breaker

Resolution:
The largest single pole available is the 30 A (QO130GFI). The largest three pole is the 50 A (QO350GFI).

The largest 2p available is a 60 A. For 2 wire loads with no neutral, the part number is QO260GFI. For 3 wire loads with a neutral, the part number is QO260GFI3W.

Schneider Electric USA