ISSUE
``x`` and ``/`` meaning in the voltage designations on the nameplate of a single phase transformer
PRODUCT LINE
Low Voltage Transformers
ENVIRONMENT
Single Phase
CAUSE
Terminology and product features
RESOLUTION
The ``x`` means ``or`` and the ``/`` means ``and``
WARNING: You cannot connect an ``x`` winding for single phase three wire connection. Example: while you can connect a 120/240 winding for single phase three wire operation, a 120 x 240 winding can only be connected for either 120 or 240 and cannot be used to supply both.
``x`` and ``/`` meaning in the voltage designations on the nameplate of a single phase transformer
PRODUCT LINE
Low Voltage Transformers
ENVIRONMENT
Single Phase
CAUSE
Terminology and product features
RESOLUTION
The ``x`` means ``or`` and the ``/`` means ``and``
WARNING: You cannot connect an ``x`` winding for single phase three wire connection. Example: while you can connect a 120/240 winding for single phase three wire operation, a 120 x 240 winding can only be connected for either 120 or 240 and cannot be used to supply both.
Released for:Schneider Electric USA
ISSUE
``x`` and ``/`` meaning in the voltage designations on the nameplate of a single phase transformer
PRODUCT LINE
Low Voltage Transformers
ENVIRONMENT
Single Phase
CAUSE
Terminology and product features
RESOLUTION
The ``x`` means ``or`` and the ``/`` means ``and``
WARNING: You cannot connect an ``x`` winding for single phase three wire connection. Example: while you can connect a 120/240 winding for single phase three wire operation, a 120 x 240 winding can only be connected for either 120 or 240 and cannot be used to supply both.
``x`` and ``/`` meaning in the voltage designations on the nameplate of a single phase transformer
PRODUCT LINE
Low Voltage Transformers
ENVIRONMENT
Single Phase
CAUSE
Terminology and product features
RESOLUTION
The ``x`` means ``or`` and the ``/`` means ``and``
WARNING: You cannot connect an ``x`` winding for single phase three wire connection. Example: while you can connect a 120/240 winding for single phase three wire operation, a 120 x 240 winding can only be connected for either 120 or 240 and cannot be used to supply both.