{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the terminal lug data for ALL the 30 Amp, US and Canada, Heavy Duty Safety Switches (for example: CH221N, CH321NAWK, H321, H361 etc.)?
Issue:
Product Features

Product Line:
Heavy Duty Safety Switches

Environment:
Main lug terminal data

Cause:
Application

Resolution:
The standard lug wire range for the 30A heavy duty safety switches is (1) #12 - #6 (AL) OR  (1) #14 - #6(CU). But the switches are also rated to accept (2) #12 - #10 AL or (2) #14 - #10 CU.
NOTES:
1) 30 -100 A switches are suitable for 60 or 75 degree wires.
2) There are NO alternate lugs available, other than compression lugs and the compression lugs DO NOT allow for larger or more wires.

Schneider Electric USA