{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Does the type of conductor used within an isolated power system (IPS) make any difference?
Issue:
Installation/setup

Product Line:
Hospital Isolated Power Systems

Environment:
NFPA99, NEC517.160

Cause:
Using the proper wire for an isolated power system is important: 1)  in order to comply with NEC insulation color requirements, as well as 2)  to have a functioning system with minimal hazard current.

Resolution:
Yes, the type of conductor used in an isolated power system (IPS) matters.  The NEC mandates special coloration for the insulating jacket of the conductor.  We also recommend a specific wire type for its insulating characteristics.  Please note the following two details:

1.  Special color:  NEC 517.160 (A) (5) Conductor Identification.
The isolated circuit conductors shall be identified as follows:
(1) Isolated Conductor No. 1 — Orange with at least one distinctive colored stripe other than white, green, or gray along the entire length of the conductor
(2) Isolated Conductor No. 2 — Brown with at least one distinctive colored stripe other than white, green, or gray along the entire length of the conductor

2.  Schneider Electric recommends using cross-linked, polyethylene wire with a dielectric constant of 3.5 or less  The mostly widely available wire for this application is low-leakage wire type XHHW or XHHW-2.

Schneider Electric USA