undefined [object Object]
{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can a 13.8kv primary transformer be connected on a wye and/or a delta system?
Issue:
Is a 13.8kv primary, MV transformer, be used for a wye and/or a delta system ?
  
Product Line:
MV Transformers
 
Environment:
Dry or Liquid Filled
  
Cause:
System Connection
  
Resolution:
A 13.8 kV Delta Primary may be used on either a Delta Source or a Wye Source.  If used on a Wye Source, the Source Neutral would not be carried through to the Transformer Primary.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top