Issue:
What is the proper procedure to follow when removing a Tesys LC1D09, LC1D12, LC1D18, LC1D25, LC1D32, or LC1D38 contactor from DIN rail?
Product Line:
IEC contactors
Environment:
TeSys D-Line
Cause:
Product Maintenance
Resolution:
To remove a D-line contactor from DIN rail the following steps must be followed while facing the front of the contactor where the terminal markings can be read.
1. With both hands, grip both the sides of the contactor placing the finger-tips over the top and thumb-tips underneath.
2. Firmly press the contactor downward towards the floor.
3. While firmly pressing the contactor downward towards the floor, pull the bottom end of the contactor outward, away from the DIN rail.
What is the proper procedure to follow when removing a Tesys LC1D09, LC1D12, LC1D18, LC1D25, LC1D32, or LC1D38 contactor from DIN rail?
Product Line:
IEC contactors
Environment:
TeSys D-Line
Cause:
Product Maintenance
Resolution:
To remove a D-line contactor from DIN rail the following steps must be followed while facing the front of the contactor where the terminal markings can be read.
1. With both hands, grip both the sides of the contactor placing the finger-tips over the top and thumb-tips underneath.
2. Firmly press the contactor downward towards the floor.
3. While firmly pressing the contactor downward towards the floor, pull the bottom end of the contactor outward, away from the DIN rail.
Released for:Schneider Electric USA
Did this answer your question?