{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
SDS Safety Data Sheet and MSDS Material Safety Data Sheet for PJC7201 electric joint compound
Issue:
SDS Safety Data Sheet and MSDS Material Safety Data Sheet for PJC7201 and PJC8311 electric joint compound

Product Line:
I-Line Circuit Breakers, QMB Plug-On Units, or Model-V MCC Units

Resolution:
See the attached SDS and MSDS below.

Other information:
I-Line™ circuit breakers, I-Line busway plug-on units, I-Line panelboards and switchboards, QMB plug-on switches, and motor control center plug-on units are supplied with factory-applied joint compound on the plug-on connectors.  The compound should not be removed because it contributes to the overall performance of the connection.  Whenever one of these units is removed and reinstalled, the joint compound should be reapplied. Catalog number PJC 7201 is a two-ounce container of compound specially formulated for the I-Line, QMB, and motor control center connections.  No other type of commercially available joint compound should be used.

Schneider Electric USA

Attachment(s)
PJC8311 MSDS.pdf [88.62 KB]
PJC7201MSDS Sanchem.pdf [110.53 KB]
PJC7201 SDS.pdf [109.19 KB]
PJC7201MSDS.pdf [132.83 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: