{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How do you cross an FAL style Mag-Gard breaker to PowerPacT?
FA type Mag-Gard motor circuit protectors (MCPs) can be replaced by PowerPacT MCPs, but there are some important differences. These two families of breakers have different dimensions, connection points, and accessories. Because of this, the equipment they are in will usually require some modification and, in some cases, replacement of the equipment will be necessary. Please see attached for the different dimensions.
The best cross for legacy FA type MCP to PowerPacT MCP are as follows:
LegacyPowerPacT
FAL3600311M HJL36030M71
FAL3600712M HJL36030M71
FAL3601513M HJL36030M71
FAL3603013M HJL36030M71
FAL3603015M HJL36030M71
FAL3605014M HJL36050M72
FAL3605016M HJL36050M72
FAL3610016M HJL36100M73
FAL3610018M HJL36100M73
FAL3615024M HJL36150M74

Sizing is not the same and replacement will not work with existing handle operator. If in an MCC, replace the complete bucket.
FAP  . . . crosses to HJP . . .
FAP . . . MT crosses to HJM . . .
FAF  . . . crosses to HJF . . .

Schneider Electric USA

Attachment(s)
FAL Dimensions.pdf [104.26 KB]
Powerpact H and J Dimensions.pdf [2.75 MB]