undefined undefined
{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
NQ main lugs only panelboard labels are upside down
Issue:
Labeling on NQ Main Lugs Panelboard

Product Line:
Panelboards

Environment:
UL 67, UL 50, CSA C22.2 No.'s 20-M1989 & 94-M91, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2003 IBC, NFPA 5000, ASCE/SE17

Cause:
A change in direction of feed for NQ main lugs only panelboards may result in upside down labels.

Resolution:
There are three labels on the dead front of an NQ main lugs only panelboard.

There is a blue identifying NQ label, which is affixed to the branch breaker portion of the dead front.  Although this label cannot be removed, the branch breaker portion of the dead front is fully symmetrical, and it can be disassembled from the adjacent dead front components to which it is attached, rotated, and then reattached so that the blue identifying label is right-side-up and readable.

The other two labels, the Danger and Warning labels are affixed to the main lug cover portion of the dead front.  The Danger and Warning labels are pre-attached in all ready-to-install interiors so that they are readable/right-side-up when the interior is oriented for bottom feed.  Although the ready-to-install interior (and any factory assembled interior configured for bottom feed) may be inverted in the field for top feed, these two labels will then be upside down.  Replacement labels can be obtained.  Order replacement label kit # PKDGWG
It contains one of each.

Schneider Electric USA

NQ main lugs only panelboard labels are upside down
Issue:
Labeling on NQ Main Lugs Panelboard

Product Line:
Panelboards

Environment:
UL 67, UL 50, CSA C22.2 No.'s 20-M1989 & 94-M91, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2003 IBC, NFPA 5000, ASCE/SE17

Cause:
A change in direction of feed for NQ main lugs only panelboards may result in upside down labels.

Resolution:
There are three labels on the dead front of an NQ main lugs only panelboard. 

There is a blue identifying NQ label, which is affixed to the branch breaker portion of the dead front.  Although this label cannot be removed, the branch breaker portion of the dead front is fully symmetrical, and it can be disassembled from the adjacent dead front components to which it is attached, rotated, and then reattached so that the blue identifying label is right-side-up and readable. 

The other two labels, the Danger and Warning labels are affixed to the main lug cover portion of the dead front.  The Danger and Warning labels are pre-attached in all ready-to-install interiors so that they are readable/right-side-up when the interior is oriented for bottom feed.  Although the ready-to-install interior (and any factory assembled interior configured for bottom feed) may be inverted in the field for top feed, these two labels will then be upside down.  Replacement labels can be obtained.  Order replacement label kit # PKDGWG
It contains one of each.

Schneider Electric USA

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range: