{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can you get both a shunt trip and UVR on a Powerpact H, J, L, M, P, or R frame circuit breaker?
Issue:
Is it possible to install both a shunt trip (MX) and an undervoltage release (MN) in a Powerpact H, J, L, M, P, or R frame breaker?

Product Line:
Molded case circuit breakers

Resolution:
No, Powerpact circuit breakers can accept only one shunt trip or one UVR (undervoltage release).
However, you can use an UVR to get both shunt trip and UVR functionality as follows:

  1. Install a UVR in the breaker
  2. Supply it from the control power source, going through NC (normally closed) contacts on a relay.  This gives you the UVR function plus a means to open the circuit as you would with a shunt trip
  3. To obtain the shunt trip function, supply the relay coil from a switched control power source as you would a shunt trip.  When you activate the switch and energize the relay coil, the NC contacts open, dropping voltage to the UVR, tripping the breaker.

Schneider Electric USA