{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is the ION 8600 meter obsolete?

Issue:
When a distributor searches an ION 8600 meter part number in "MySchneider" the part number will show up as obsolete.

Product Line:
ION 8600, ION 8650

Environment:
Device obsolete, device replacement

Cause:
ION 8600 and ION 8650 meters are now both ISO CAL certified, therefore ION 8600 will no longer be sold.

Resolution:
If a distributor or customer contacts technical support requesting information regarding purchasing an ION 8600, please recommend an ION 8650 meter and let the customer know that the ION 8600 meter is obsolete.

The ION 8650 meter is ISO CAL certified.

Attached file shows ISO Approved Meters.

Schneider Electric USA

Attachment(s)
ApprovedISOMeters.pdf [185.94 KB]