Search FAQs
What is the difference between a XACA03 AND XACA03H7?
Issue:
What does the H7 suffix mean on XACA03H7?
Product Line:
Push Buttons and Operator Interface
Environment:
22m XACA pendant station. All XACA pendant stations
Cause:
Wants to clarify the difference between with and without the H7 on the end of the part number.
Resolution:
There is no difference between the 2 parts. H7 is a country code for the North American market. Units with this country code will be UL and CSA marked and have 1/2 inch NPT conduit entry, if they have one. The H7 has always been on the part number, but was transparent when ordering in the US. Schneider has decided to put the country code back on the part number so world wide units are identified in the same way.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: