Issue:
ABL8 power supplies mounting
Product Line:
Phaseo power supplies
Environment:
North America
Resolution:
The term vertical mount means the device must be mounted upright on a vertical mounting plane. The writing
on the device and labels are legible and are in the proper orientation (cannot be upside down).
The power supply needs to vertical because of cooling down and venting for the device. If the power supply
is mounted differently, the device will not cool down properly and reduce the life of the device or the device can
overheat and be damaged.