{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the maximum mounting distance for remote mounting a graphic display (HMI VW3A1101) on the ATV61/71?

Issue:
Needs the max mounting distance for remote mounting a graphic display (HMI VW3A1101) on the ATV61/71

Product Line:
ATV61 ATV71

Environment:
All

Cause:
Need mounting distance of 150 ft from the VFD

Resolution:
We do not have a offering or configuration available at that distance.
The max cable length we offer for the VW3A1101 is 10 meters
1 meter length VW3A1104R10
3 meter length VW3A1104R30
5 meter length VW3A1104R50
10 meter length VW3A1104R100

However, attached is a configuration that was successfully used by one of our customers up to 200 ft.

Schneider Electric USA

Attachment(s)
ATV71 IP54 remote mount.pdf [229.29 KB]
ATV71 IP65 remote mount.pdf [219.53 KB]