{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the catalog numbers and purpose for wire harnesses for Powerpact H, J, and L frame circuit breakers?
Issue:
What is the purpose of optional wiring harnesses in the Powerpact H Frame, J Frame and L Frame breakers in both Unit Mount and ILINE applications, and what are the catalog numbers?

Product Line:
Powerpact H Frame, Powerpact J Frame, and Powerpact L Frame

Resolution:
The wiring harnesses for the H, J, and L Frame breakers allows the accessory wiring to exit the circuit breaker through wiring channels in the side of the circuit breakers. This feature is especially important in I-line application because I-line bussing restricts the control wire from coming out the top of the breaker.  I-line wire harness is included as standard for communication network accessories. Wire harnesses may also be used for unit mount applications.

Suffix
Harness2
Kit No.
YH3
ZSI Wire Harness, H/J Frame
S434300
YH3
ZSI Wire Harness, L-Frame
S434301
YH2
ENCT Wire Harness
S434302
YH1
OF Wire Harness
S434500
YH1
SD/SDE Wire Harness
S434501
YH1
SDx/SDTAM Wire Harness
S434502
YH1
MN Wire Harness
S434503
YH1
MX Wire Harness
S434504
YH1
Motor Operator Wire Harness
S434506
YH1
Communicating Motor Operator Wire Harness
S434507
YH13
NSX Wire Harness
S434508
YH4
ENCT and ZSI Wire Harnesses
YH13
24 Vdc Power Supply Wire Harness
S434505
2YH1 = all installed accessories but ZSI and ENCT
YH2 = ENCT and all installed accessories
YH3 = ZSI and all installed accessories
YH4 = ZSI, ENCT and all installed accessories
3I-Line wire harness included for communication network accessories.
Optional wire harness for unit mount requires YH1 suffix.

Note:  As indicated in the product selector, the wire harness is automatically included with communication accessories without YH1 suffix. Wire harness must be selected for other electrical accessories.

See instruction bulletin, S1A80378

Schneider Electric USA

What are the catalog numbers and purpose for wire harnesses for Powerpact H, J, and L frame circuit breakers?
Issue:
What is the purpose of optional wiring harnesses in the Powerpact H Frame, J Frame and L Frame breakers in both Unit Mount and ILINE applications, and what are the catalog numbers? 

Product Line:
Powerpact H Frame, Powerpact J Frame, and Powerpact L Frame

Resolution:
The wiring harnesses for the H, J, and L Frame breakers allows the accessory wiring to exit the circuit breaker through wiring channels in the side of the circuit breakers. This feature is especially important in I-line application because I-line bussing restricts the control wire from coming out the top of the breaker.  I-line wire harness is included as standard for communication network accessories. Wire harnesses may also be used for unit mount applications.

 
Suffix
 Harness2 
 Kit No.
 YH3
 ZSI Wire Harness, H/J Frame
 S434300
 YH3
 ZSI Wire Harness, L-Frame
 S434301
 YH2
 ENCT Wire Harness
 S434302
 YH1
 OF Wire Harness
 S434500
 YH1
 SD/SDE Wire Harness
 S434501
 YH1
 SDx/SDTAM Wire Harness
 S434502
 YH1
 MN Wire Harness
 S434503
 YH1
 MX Wire Harness
 S434504
 YH1
 Motor Operator Wire Harness
 S434506
 YH1
 Communicating Motor Operator Wire Harness
 S434507
 YH13
 NSX Wire Harness
 S434508
 YH4
 ENCT and ZSI Wire Harnesses
 
 YH13
 24 Vdc Power Supply Wire Harness
 S434505
 
2YH1 = all installed accessories but ZSI and ENCT
 YH2 = ENCT and all installed accessories
 YH3 = ZSI and all installed accessories
 YH4 = ZSI, ENCT and all installed accessories
3I-Line wire harness included for communication network accessories.
 Optional wire harness for unit mount requires YH1 suffix.

Note:  As indicated in the product selector, the wire harness is automatically included with communication accessories without YH1 suffix. Wire harness must be selected for other electrical accessories.

See instruction bulletin, S1A80378

Schneider Electric USA

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top