Issue:
Needs to Identify the max electrical ratings for the NSYTRV22 terminal block.
Product Line:
Linergy TR Screw terminal blocks.
Environment:
Linergy TR NSYTRV22, NSYTRV22BL, NSYTRV22AR, NSYTRV22RD, NSYTRV22WH
Cause:
To clarify the electrical ratings for the new line of terminal blocks compared to the old AB1 terminal blocks.
Resolution:
Terminal block NSYTRV22** have the following ratings:
UL 600V, 20A
CSA 600V, 20A
ATEX 690V, 22A
All of the ratings and accessories for this terminal block is found on page 20 in the LINERGY CATALOG 9080CT1301.