{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the electrical ratings for NSYTRV42 terminal block?

Issue:
Needs to Identify the electrical ratings for the NSYTRV42 terminal block.

Product Line:
Linergy TR Screw terminal blocks.

Environment:
Terminal Blocks

Cause:
To clarify the electrical ratings for the new line of terminal blocks compared to the old AB1 terminal blocks.

Resolution:
Terminal block NSYTRV42** have the following ratings:
UL 600V, 30A
CSA 600V, 30A
ATEX 690V, 30A.

All of the ratings and accessories for this terminal block is found on page 20 in the LINERGY CATALOG 9080CT1301.

Schneider Electric USA

Attachment(s)
LINERGY PAGE 20.pdf [115.1 KB]