{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: Can the I-Line™ Combination panels be used with different voltage systems within the same panel, ie 480V for the I-Line™ portion and the other panels at 208V?

Issue:
Can the I-Line™ Combination panels be used with different voltage systems within the same panel, such as 480V for the I line portion and the other panels at 208V?

Product Line:
I-Line™ Combo Panelboards

Environment:
All models

Resolution:
The panels have to be all one voltage system and cannot be mixed. The following video demonstrates why I-Line™ Combo Panelboards utilize a single-source voltage system within single panels.

Schneider Electric USA

Attachment(s)
2013 I Line Combo panel catalog .pdf [1.96 MB]