{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: How does the cover open on the L600AWK and L600AWKMC circuit breaker enclosures?
Issue:
Product feature

Product Line:
CB Enclosure

Resolution:
The cover is hinged to the enclosure on the left side, so it opens from right to left. But since this is a NEMA 12 enclosure, there are some brackets on the right side of the cover and enclosure and the cover physically bolts to the enclosure on the right side. To open the cover, these bolts will need to be loosened and the operating handle will need to be in the off position.

To open the cover if the operating handle is in the ON position, all the bolts will need to be loosened and the cover interlock defeat mechanism will need to be operated for the cover to open.

Schneider Electric USA

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: