{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can a legacy MA, MH or electronic trip version (MX or ME) circuit breakers be installed in or relocated to current design (Series 2) QED I-Line distribution sections?
Issue:
Application, Installation

Product Line:
Switchboards

Environment:
NEMA PB-2, UL 891, NFPA 70 Art. 408

Cause:
Updating an older service with a new switchboard (higher ampere rating, other necessary features) often involves feeding existing circuits from the new switchboard.

Resolution:
The current design (Series 2) I-Line distribution sections of QED switchboards lack a key feature required for mounting legacy MA, MH frame circuit breakers or electronic trip versions (MX, ME) of these legacy circuit breakers:  the back pan of the Series 2 design I-Line distribution section is not punched with a cut-out for the mounting cam feature required for mounting these circuit breakers.  For this reason these legacy circuit breakers cannot be installed in or relocated to a current design (Series 2) I-Line distribution section.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.