{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are safety switches provided with visible blades?
Issue:
Feature

Product Line:
Safety Switches

Resolution:
Yes, with exception. All of our Type 1, 3R, 4/4X/5, 12/3R and 12K switches are designed so that the blades are visible with the switch in the OFF position and the cover open. Type 7/9 devices are enclosed molded case switches and do not have visible blades.

Schneider Electric USA