Issue:
Molded Case Switch Enclosure
Product Line:
Load Centers / Molded Case Circuit Breaker
Resolution:
Yes, the L600AWKMC is available for use with the PowerPacT L frame molded case switch. The enclosure is listed and labeled as rainproof and dusttight and is suitable for NEMA 1, 3, 3R, 5, or 12 installations. When used in an outdoor, rainproof application, remove the drain screw in the bottom endwall and discard.
Molded Case Switch Enclosure
Product Line:
Load Centers / Molded Case Circuit Breaker
Resolution:
Yes, the L600AWKMC is available for use with the PowerPacT L frame molded case switch. The enclosure is listed and labeled as rainproof and dusttight and is suitable for NEMA 1, 3, 3R, 5, or 12 installations. When used in an outdoor, rainproof application, remove the drain screw in the bottom endwall and discard.
Released for:Schneider Electric USA