{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are dual mounted circuit breaker branch feeder units for Model 4 motor control centers available with different trip ratings for the circuit breakers (within the frame size)?
Issue:
Dual mounted circuit breaker branch feeder units for Model 4 MCC's with different trip ratings

Product Line:
PTEQP - LV EQPT (IEC & NEMA)

Environment:
NEMA ICS 18-2001, EEMAC, UL 845, NFPA70 Art. 430

Cause:
Dual circuit breaker branch units save mounting space in a motor control center; however, the desired trip rating may not be identical for the two circuit breakers.

Resolution:
The offer of dual branch feeder units in the past had a break at 50A.  Dual feeder units with both circuit breakers rated 50A and below were offered, and above 50A trip (up to 100A maximum) could be grouped together in a dual feeder unit.  This was due to the connection to the vertical bus of the MCC section.

Presently mixed ampere ratings for dual circuit breaker feeder units are available, and a 50A break point no longer applies.  A 15A/100A unit, for example, could be ordered.  The maximum available ampere rating is still 100A.  Also, the Powerpact H breakers, not the legacy FH circuit breakers are furnished.  The special mixed ampere rating dual branch feeder units must be quoted by and ordered from the local Schneider Electric USA field office.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.