{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are there replacement parts for the MD enclosed switches?

Issue:
Is the Interior Replaceable in the MD Motor Disconnect Switches MD3304X and MD3604X?

Product Line:
Disconnect Switches

Environment:
Motor disconnect switch

Resolution:
Replacement interiors for these switches are not available. The only accessory parts available are as follows:
MDS30P, Add-on power pole.
MDSAN20, Auxiliary contacts (2) normally open.
MDSAN11, Auxiliary contacts (1) normally and (1) normally closed.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.