Search FAQs
On an IGD display, what does 9.5 error code mean?
Issue:
Error code 9.5 on LIM
Product Line:
Medical Equipment
Environment:
IGD
Cause:
Troubleshooting
Resolution:
This is a line ratio problem. Make sure the internal DIP switch is not in the 3ph position if panel is 1 phase. If it is in the 1 ph position , replace the LIM.
Error code 9.5 on LIM
Product Line:
Medical Equipment
Environment:
IGD
Cause:
Troubleshooting
Resolution:
This is a line ratio problem. Make sure the internal DIP switch is not in the 3ph position if panel is 1 phase. If it is in the 1 ph position , replace the LIM.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: