{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are ANY of the QO OEM mounting bases UL Listed or CSA Certified?
Issue:
Standards

Product Line:
OEM Mounting Base

Resolution:
The QO OEM mounting bases are considered UL Recognized Components in the UL File E6294 and a CSA Panelboard Interior in CSA File LL89066 to be used by OEMs when the bases are incorportated into their equipment. The final acceptance of these bases is dependant upon the installation and use in the complete equipment submitted to UL or CSA by the OEM.

Schneider Electric USA

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: