{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How much inrush current can a square D NEMA starter handle?
Issue:
My motor inrush in higher than the continuous current rating of my NEMA starter - how much inrush can the starter handle?

Product Line:
All Schneider Electric products

Environment:
Products sold and used in the United States

Cause:
Motor inrush is higher than continuous current rating.


Resolution:
Per NEMA the motor starter has to be able 10 times the continuous current on inrush. For example, if the continuous current rating is 9 amps, the NEMA motor starter must be rated for 90 amps of inrush from the motor.

Schneider Electric USA