Issue:
What are the VA coil values for the 8903S contactors?
Product Line:
8903S Lighting Contactors
Environment:
Us Product
Cause:
These values are not published on the standard data sheets
Resolution:
8903SM - 245VA inrush - 27VA sealed
8903SP - 311VA inrush - 37VA sealed
8903SQ - 700VA inrush - 46VA sealed
8903SV - 1185VA inrush - 85VA sealed
8903SX - 2970VA inrush - 212VA sealed
What are the VA coil values for the 8903S contactors?
Product Line:
8903S Lighting Contactors
Environment:
Us Product
Cause:
These values are not published on the standard data sheets
Resolution:
8903SM - 245VA inrush - 27VA sealed
8903SP - 311VA inrush - 37VA sealed
8903SQ - 700VA inrush - 46VA sealed
8903SV - 1185VA inrush - 85VA sealed
8903SX - 2970VA inrush - 212VA sealed