{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How many Nema 1 starter buckets can be put into a single section of a Model 5/6 MCC ( Motor Control Center)
Issue:
Amount of 12" High Nema 1 starter buckets that can be put into a single section of a Model 6 MCC ( Motor Control Center)

Product Line:
Model 6 Motor Control Centers

Environment:
Layout/Quoting

Cause:
Clarification of Lineup sections

Resolution:
A Qty of (6) 12"H starter buckets can be place in one MCC section for 72" of total bucket space /per section allowed.
MCC Layout Instructions

Schneider Electric USA