{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: What is the mounting hardware kit required to mount a breaker inside I-Line® panel board?
Issue:
How to mount a breaker inside an I-Line panel board?

Product Line:
Circuit breakers
I-Line panel boards

Resolution:
I-Line breakers can be installed inside an I-Line panel board without the need for additional mounting hardware. I-Line breakers have the I-Line connector on the line side which directly connects to the bus bar inside the panel board, as well as the mounting screw on the bottom.

 

 

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top