{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Replacing IEC contactor in reversing set

Issue:
Can the LC1D contactor be replaced in an LC2D reversing set?  Will additional pieces/accessories be necessary?

Product Line:
IEC Contactors and Starters

Environment:
Tesys D Contactors

Cause:
Occasionally one unit in a pair must be replaced.

Resolution:
So long as the contactor being replaced is the exact same model with the exact same coil voltage, an individual unit can be replaced with no additional equipment.

Schneider Electric USA