{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What Combination Service Entrance Devices (CSED) can the SR69064A Solar Ready Kit be used with?
Issue:
SR69064A Solar Ready Kit used with Combination Service Entrance Devices (CSED).

Product Line:
CSED

Resolution:
See below all the Current Design Combination Service Entrance Devices(CSED) that will allow the use of the Solar Ready Kit part #SR69064A.
The Solar Ready kit is only a set of Lugs that can be installed on the Line Side of the Service Disconnect to allow a solar feed into the panel to meet certain aspects of the NEC. PLEASE SEE THE NEC FOR APPROPRIATE APPLICATIONS

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.