{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How to upgrade firmware of PM5xxx meter even though DLF3000 will apparently not accept a broadcast ID of 255
Issue
Customer might not be able to add he meter in DLF because the highest ID it would take is 247, and the hardcoded ID for the PM5XXX is 255

Product Line
PM5000 series

Environment
Performing firmware upgrade for the PM5XXX

Cause
The highest ID DLF3000 would take is 247, and the hardcoded ID for the PM5XXX is 255

Resolution
See the attached document provided by the hardware department.

Schneider Electric USA

Attachment(s)
Device_Address-255_selection_through_DLF.pdf [872.88 KB]