{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Using XACS contact blocks with XACA pendant stations
Issue:
The contact block(s) XACS*** are not fitting in the enclosure behind the pushbuttons.

Product Line:
XACA pendant with XACS type contact blocks

Environment:
Maintenance/selection

Cause:
These contact blocks are sometimes mistakenly used in the wrong place.

Resolution:
These contact blocks are for a base mounted operator only.  That is they will only fit in the bottom of the enclosure to be used with an operator mounted there.  These contact blocks cannot be used with the cover mounted units

Schneider Electric USA