{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is printed on the PSDS stickers (for QO, Homeline, and CSED products)?
Issue:
On the directory circuit ID Labels or PSDS sticker, what is printed on them?

Product Line:
Load Centers and CSED

Resolution:
PSDS Stickers Nomenclature - The wording below will be provided on the PSDS stickers. The (x) preceding the nomenclature below is the quantity of stickers with that specific wording.
(1) Master Bedroom, (2) Bedroom  #1, (2) Bedroom #2, (2) Bedroom #3, (2) Bedroom #4, (2) Bedroom #5
(1) Master Bathroom, (1) Mstr Bath Rcpt, (1) Mstr Bath Lts, (2) Up Bathroom, (1) Down Bathroom, (2) Bathroom #2, (2) Bathroom #3, (2) Bathroom #4, (8) Bathroom GFCI, (1) Powder Bathroom, (1) Jack & Jill Bathroom, (1) Wall Heater
(8) AC Condenser, (5) Forced Air Unit, (1) Down Furnace, (1) Up Furnace
(5) Kitchen GFCI, (2) Kitchen, (3) 220V Oven, (1) 220V Range, (1) 220V Cooktop, (1) Range, (1) Stove, (1) Oven, (1) Wall Oven, (1) Dishwasher, (3) Freezer, (2) Refrigerator, (2) Microwave, (1) Garbage Disposal, (1) Trash Compactor
(1) Garage, (1) Garage Door, (1) Garage GFCI, (3) Central Vac, (2) Workshop
(1) Family Room, (1) Family Rm Rcpt, (1) Family Rm Lts, (1) Living Room, (1) Dining Room, (1) Den, (2) Media Room, (1) Office, (1) Bonus Room, (1) Foyer Lt and Rcpt, (4) Basement, (1) Spare Room, (1) Stereo, (1) Nook, (1) Casita
(1) Utility Room, (1) 110V Dryer, (1) 220V Dryer, (1) Dryer, (1) Clothes Washer
(2) Attic Lts, (2) Bar Lts & Rcpt, (1) Bookcase Lts, (1) Mud Room Lts, (1) Sun Room Lts
(1) 220V Spa, (1) 110V Jacuzzi Tub, (1) Sump Pump, (2) Sub-Panel, (1) Pool, (1) Play Rm Rcpt, (1) Outdoor Receptacle, (1) Smoke Detectors, (1) Dedicated Circuit, (2) Other

Schneider Electric USA

Explore more
Range:
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Category: