{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
There are two different types of pendant for each size listed, but only one is valid. Why is that?
Issue:
Identify the differences between 9001 pendant stations.

Product Line:
9001SKYP Pendant Stations

Environment:
Push Buttons and Operator Interface

Resolution:
For each size station, there are two parts - one is part of an assembled station, the other is for purchase by itself as an empty enclosure.
The parts 9001SKYP20, 9001SKYP40, 9001SKYP60, 9001SKYP80, and 9001SKYP100 cannot be ordered separately, but will be listed on a BOM as a component piece.
The corresponding parts 9001SKYP2, 9001SKYP4, 9001SKYP6, 9001SKYP8, and 9001SKYP10 are available to order seperately.
The two different part numbers refer to the exact same enclosure.

Schneider Electric USA