{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the difference between the different PME device driver suffix?
Issue:
There are device type installers for device drivers that are not natively supported in PME. They have different suffix, and it's necessary to know what how the suffix differentiates these drivers

Product Line:
Struxureware Power Monitoring Expert 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x

Environment:
Power Monitoring Expert Software Configuration

Cause:
The suffix determines what the device driver supports and which features are excluded. It's necessary to know this to determine if the device type installer will meet the requirements.

Resolution:
The image below describes what each suffix in a device type installer entails:


Schneider Electric USA