{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can GV2 manual motor starters be used with single phase motors?
Issue:
Are the GV2 Manual starters suitable to be used on single phase applications?

Product Line:
IEC Contactors and Starters

Environment:
GV2 Manual motor starters

Cause:
These units show single phase ratings, but are set up for three phase applications

Resolution:
These units need to see current across three poles to operate properly.  If only one or two legs are wired for a single phase application, the unit will trip as it will think that a phase has been dropped.  Thus, either a hot leg or the neutral must be looped through the otherwise unused pole so that all three poles are being used.

Schneider Electric USA

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: