Issue:
Product features
Product Line:
Circuit Breaker Enclosure
Resolution:
The provision to padlock the operating handle in the ON position is not standard on the L600AWK or L600AWKMC enclosures. To obtain a factory modification for lock ON provision, add the suffix SPLO to the standard catalog number.
The SPLO provision will allow the customer to use one 3/8" maximum hasp padlock to lock the switch in the ON position.
Product features
Product Line:
Circuit Breaker Enclosure
Resolution:
The provision to padlock the operating handle in the ON position is not standard on the L600AWK or L600AWKMC enclosures. To obtain a factory modification for lock ON provision, add the suffix SPLO to the standard catalog number.
The SPLO provision will allow the customer to use one 3/8" maximum hasp padlock to lock the switch in the ON position.
Released for:Schneider Electric USA