{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can the HRL or JRL circuit breakers be installed in the J250 circuit breaker enclosures?

Issue:
Application

Product Line:
CB Enclosures

Resolution:
The J250 family of enclosures will accept only the HDL, HGL, HJL, HLL, JDL, JGL, JJL, or JLL circuit breakers. The enclosures are not listed for use with the HRL or JRL circuit breakers.

We do have minimum recommended enclosure dimensions (height x width x depth) for them listed below:

HRL:
80%: 18.13 x 8.63 x 4.13 in.
100%: 62 x 22.5 x 14 in.

JRL:
80%: 28.5 x 12.38 x 5.38 in.
100%: 62 x 22.5 x 14 in.

Schneider Electric USA