{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are the Powerpact two device solution breakers with M38X suffixes UL listed?
Issue:
Are the Powerpact two device solution breakers with M38X suffixes UL listed?

Product Line:
Circuit breakers

Resolution:
Even though Powerpact motor circuit protectors with suffix M38X have thermal and short circuit protection, they are not UL 489 listed.
They are listed per UL 60947-4-1A and CSA C22.2 NO 60947-4-1-07. See attached certificate and attached faceplate label.

Schneider Electric USA

Attachment(s)
Powerpact MCP M38X -CertificateofCompliance.docx [878.92 KB]
HGL36030M38X_fp.pdf [26.1 KB]