{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are alternate lugs available for the EZM3400CB, Series M01 main device?
Issue:
Optional wire sizes

Product Line:
EZ Meter-Pak Metering Equipment

Resolution:
The Standard Mechanical Lugs for an EZM3400CB, Series M01 include:
The Factory installed Main Circuit Breaker LHP36400 is supplied with the following Standard Lugs:
To accommodate: (1) 1/0 AWG to 600 kcmil OR (2) 1/0 AWG to 250 kcmil AL/CU Wires per Phase using (1) AL400LA Lug Kit per Phase(per pole).
The Line Side Neutral Assembly is supplied with the following Standard Lugs:
To accommodate: (1) 1/0 AWG to 600 kcmil OR (2) 1/0 AWG to 250 kcmil AL/CU Wires using (1) MMLK250 Lug Kit (Kit includes 3, 2-Barrel Lugs, only 1 of these 3 Lugs can be installed on the neutral)

The Alternate Lugs for the EZM3400CB, Series M01 include;
To accommodate (1) 750 kcmil Al/Cu wire Per phase for the Main breaker, need to use lug kit AL400LH7. This lug kit includes only ONE lug, so for the 3pole main breaker, need to order 3 Kits.
To accommodate (1) 750 kcmil Al/Cu wire for the Main Neutral, need to use (1) EZMSK2 Lug Landing Kit(purchase separately) and (1) TA8002N ILSCO Lug (purchase separately).
NOTE: the EZMSK2 kit comes with 4 - lug landing pads and the Main Neutral will ONLY accept 1 pad and 1 lug.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: