undefined undefined
{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the termination temperature rating for HVL/cc?
Issue:
HVL/cc termination temperature

Product Line:
INMVP - PRODUCT_SWITCHGEAR

Environment:
NEMA, UL, ANSI/IEEE C37.20.3, C37.20.4, C37.57, C37.58, CSA 22.2 no.s 31 and 193

Cause:
Proper selection and sizing of conductors.

Resolution:
The lugs and terminations for HVL/cc are rated 90 deg C. Cable rated 105 deg C may be used; however, it will have to be sized as if it were 90 deg C.

Schneider Electric USA

What is the termination temperature rating for HVL/cc?
Issue:
HVL/cc termination temperature

Product Line:
INMVP - PRODUCT_SWITCHGEAR

Environment:
NEMA, UL, ANSI/IEEE C37.20.3, C37.20.4, C37.57, C37.58, CSA 22.2 no.s 31 and 193

Cause:
Proper selection and sizing of conductors.

Resolution:
The lugs and terminations for HVL/cc are rated 90 deg C. Cable rated 105 deg C may be used; however, it will have to be sized as if it were 90 deg C.
 

Schneider Electric USA

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range: