{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can a 8998SBF060 be used in a MCC5?
Issue:
Model 6 breaker bucket in MCC5

Product Line:
Motor Control Centers

Environment:
MCC5

Cause:
Fit and Application

Resolution:
Yes, they will also need a midshelf part number 8045086550. This cannot be installed in the top location of any section on the Model 5 MCC.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.