Search FAQs
Is there a flush mount kit available for the HEPD80 surge protective device?
Issue:
What is the part number of flush mount kit for the HEPD80 and/or HEPD50 surge protective device?
Product Line:
Surge Protective Devices
Environment:
Installation
Cause:
Product Features
Resolution:
There are 2 flush mount kits available for HEPD.
HEPD80MKF - Flush mount kit for the old HEPD80 which is colored gray.
HEPD58MKF - Flush mount kit for the current HEPD80 and HEPD50 which are both colored white.
What is the part number of flush mount kit for the HEPD80 and/or HEPD50 surge protective device?
Product Line:
Surge Protective Devices
Environment:
Installation
Cause:
Product Features
Resolution:
There are 2 flush mount kits available for HEPD.
HEPD80MKF - Flush mount kit for the old HEPD80 which is colored gray.
HEPD58MKF - Flush mount kit for the current HEPD80 and HEPD50 which are both colored white.
Released for:Schneider Electric USA
Explore more
Product:
Explore more
Product: