{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can an NF panel be run on 380V?
Issue:
NF Panel running correctly on 380V system

Product Line:
Circuit breakers, Panelboards

Environment:
NF Panelboard

Cause:
Can the NF panel board be used on a 380V system.  Not a normal voltage in US.

Resolution:
380Y/277V is a valid international voltage for the NF panelboard.
To achieve the panel nameplate to read 380Y/277V, the panel must be built as factory assembled and configured with that voltage.

Schneider Electric USA