undefined undefined
{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What does letter 'M' or 'K' represent on front display of ION7300 series meters?
Issue
When reading a value from the front display of an ION 7300 series meter, and 'M' or 'K' is shown in the number. For example, KWh rec value is reading 1M225 as shown below. 

ION7300 Display

Product Line
ION7300 series meter

Environment
Meter Front Display

Cause
The meter display is configured to show more than one parameter and does not have enough space to show all the digits. As a result, the meter rounds up the “1255922.75” to “1M225” or “255940” to “255K9” on display; where M stands for Million, and K stands for Killo.  

Resolution:
In order to see all digits, the display can be configured to show only the desired parameter as shown below.

Digits
 
Follow steps below in order to configure meter's display to show only one parameter on screen:
  • Connect to the meter using ION Setup. 
  • Switch to the Advanced Mode and navigate to the Display Modules folder. 
  • Right click on the Display Module to be configured and remove undesired parameters from the Input tab. 
 

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: