{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
For Powerpact H, J, L, and P frame breakers with rotary operated handles, are individual components of the rotary handle available separately?
Issue:
Can I get just the shaft for a rotary handle?

Product Line:
Circuit Breakers

Resolution:
For Powerpact H, J, L, and P frame breakers with the rotary operated handles shown below, individual components of the rotary handle are not available as separate items. Instead, order a complete rotary handle kit.
  • Powerpact H, J, L and P frame breakers with suffix RD10, RD12, RD13, RD16, RD20, RD22, RD23, RE10, RE13, RE16, or RE20
  • Rotary operated handle kits S29337, S29338, S29339, S29340, S32597, S32598, S32599, S32600, S33875


Schneider Electric USA