{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Does Square D offer the Homeline load center covers painted 'White' instead of the standard gray cover?

Article available in these languages: Spanish

Issue:
Product Design features

Product Line:
Homeline Load Centers

Environment:
Paint

Cause:
Application

Resolution:
Yes. Most of the Homeline load center covers are available in what is called an 'Appliance White' (this is basically a Semi-gloss finish white). For a catalog number just add the suffix 'W' to the standard cover catalog number, for example HOMC30UCW. Since the Homeline load centers are provided with a gray combination cover as a standard feature, purchasing a white cover separately will result in an unused gray cover. All the available white cover catalog numbers are loaded in the Q2C system with pricing and lead times. Some catalog numbers will have minimum quantity restrictions.

Available catalog numbers of Homeline covers painted white are:
HOMC8UCW
HOMC12UCW
HOMC16UCW
HOMC20UCW
HOMC20U100CW
HOMC24UCW
HOMC30UCW
HOMC30U125CW
HOMC40UCW

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: