{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are key interlocks or provisions for a field installed key interlock available for general duty, heavy duty, or double throw safety switches?
Issue:
Product design features

Product Line:
Safety Switches

Resolution:
Key interlocks are NOT available for the General Duty Safety Switch product line.

Key interlocks are ONLY available factory installed for the Heavy Duty Safety Switches, 30 to 1200 A, NEMA 12 and 4X (304 grade stainless steel)
The key interlocks are NOT available for NEMA 1, 3R, Fiberglass or Krydon switches, and no provisions for field installation are available on any safety switches.

Key Interlocks are ONLY available factory installed for the Double Throw Safety Switches, 30 to 200 A, NEMA 12 and 4X(304 grade stainless steel).
NOTE: Key interlocks are NOT available for ANY of the NEMA 1 or 3R. The Key interlocks are NOT available for any of the 400amp and 600amp Double Throw Safety Switches, the following catalog numbers: DTU225, DTU225R, DTU325, DTU325R, DTU365, DTU365R, DTU365DS, DTU365AWK, DTU465, DTU465R,  DTU326, DTU326R, DTU426, DTU426R, DTU366, DTU366R, DTU366AWK, DTU466 and DTU466R


Schneider Electric USA

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: